10/23/2020 1:54 PM | |
Joined: 9/14/2020 Last visit: 11/2/2021 Posts: 3 Rating: (0) |
Hello An error shows during installation of TIA Portal V15.1 (it includes Update 5) on Windows 10. I attach log file with description of error. After installation it is possible to open TIA Portal, but it crashes when I try to add new device to the project. I've disabled anti-virus and firewall software. Any more suggestions? BTW, I had to move installation files to c:\TIA folder from default folder, because VC Redistributable couldn't install from default folder (probably path was too long). Best regards Marcin AttachmentSIA_STEP_7_PRO_WINCC_ADV_V15.1_Upd5@20-10-23_11-40-20_summary.txt (233 Downloads) |
Last edited by: MarcinAK at: 10/23/2020 15:04:25Clarification |
|
Follow us on