11/16/2020 6:38 PM | |
Joined: 9/23/2005 Last visit: 6/26/2024 Posts: 4347 Rating: (1436)
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Trends controls presents values in time axis. E.g. the tags are collected at a fixed time base basis. However, the data could be collected on demand, that means, triggered by an auxiliar variable change. It could be useful for synchronize the PLC data with the trend (the read should be done at a determinate production point and not at fix time bases). This simple sample show how to configure it. TIP: This application example is an extension of the use of trends. An example of how to configure Trend objects is showed in the post "WinCC Unified – Simple Sample - Trends (time based)" (https://support.industry.siemens.com/tf//ww/en/posts/wincc-unified-simple-sample-trends-time-based/226107/?page=0&pageSize=10). Configuration main steps:
Simple sample program (zipped / archived). AttachmentProject.zip (800 Downloads) |
Denilson Pegaia |
|
Follow us on