5/4/2012 6:54 PM | |
Posts: 8946 Rating: (999) |
Is it possible that you use the wrong back-up file? |
5/4/2012 7:58 PM | |
Posts: 8946 Rating: (999) |
Is the spare OPconnected to the PLC? If not, may be you should try so...? |
5/4/2012 8:27 PM | |
Posts: 7 Rating: (0) |
I dont have the source file, no. |
5/4/2012 8:43 PM | |
Posts: 8946 Rating: (999) |
Perhaps, the buffer battery is empty, if one is installed. please check: http://support.automation.siemens.com/WW/view/en/28971044 But, honestly, I have no Idea if the battery can do the problem you describe... |
Follow us on