10/4/2019 2:18 PM | |
Posts: 1 Rating: (0) |
Good evening to all. I'm using WindowsXP SP3 and WINCC 7.0 I've just set the autolog into system registry and it works. I've made a "batch" script that start a WINCC project (SCADA) with the AutostartRT that works perfectly. The problem is that : 1. When I run script with the explorer.exe shell set on, it works fine and it's fast.2. When I run script instead of the explorer.exe shell, the AutostartRT is very slow, and CCUCSurrogate.exe process is blocking constantly. I performed a test: When I start it withot explorer.exe shell, it's slow, but during startup if I run the explorer.exe shell, the project startup became fast. is there anybody who have solved this problem? Pietro Montieri ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/04/2019 15:18:02New subject after splitting |
|