12/8/2011 9:45 AM | |
Posts: 8 Rating: (1) |
Hello! Have the following problem: I've configured OS station, CAS station, activated my project on them both, but the folder ArchiveDir is still empty! Becides, if the CAS project is deactivated, WinCC Server makes backup to the folder ArchiveDir normally, so I made conclusion that the Network is OK. But the CAS project have to be activated according to datasheet. How can I get my archives? What is wrong with my net? Server: WinCC 7.0 SP2 Windows XP SP 3 CAS : WinCC 7.0 SP2, WinCC CAS 7.0 SP2 Windows Server 2008 Computer names in project: OS Server - Maslo OS Client (not connected) - Soya ES - Zeff CAS - Win AttachmentScreens.zip (126 Downloads) |
12/9/2011 7:51 AM | |
Posts: 8 Rating: (1) |
And one more question: What Server roles must be swithed on on the CAS Server? Can this be a problem why my Net works wrong? |
12/12/2011 11:35 AM | |
Posts: 1530 Rating: (59)
|
Hello Cutecat, |
This contribution was helpful to1 thankful Users |
12/15/2011 10:48 AM | |
Posts: 1530 Rating: (59)
|
Hello Cutecat, today I have been looking again into manual of CAS, in hope to find out, what could be your problem. Could it be, that you copied whole WinCC project to your CAS, because in manual I found following:
As I haven't been working with CAS in detail, I can only try to find out something, if I use all my other experiences with WinCC in the back of my head Hoping I could help you Bizur |