12/5/2011 11:53 AM | |
Posts: 40 Rating:
|
IS IT POSSIBLE TO CONFIGURE A KTP600 PN Basic HMI WITH LOGO OBA7, WITH OUT S7 |
12/5/2011 12:33 PM | |
Posts: 13 Rating:
|
HI When using a panel with the LOGO 0BA7 you still need to configure the panel with its own software. For Siemens panel WinCC Flexible or WinCC |
12/5/2011 3:11 PM | |
Posts: 6 Rating:
|
Hello Take a look here,there are some information how u can do it. http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=56348902&caller=nl |
Last edited by: stivk at: 12/5/2011 3:12 PMLast edited by: stivk at: 12/5/2011 3:11 PM |
|
12/6/2011 6:21 AM | |
Posts: 40 Rating:
|
Thankyou for your replies, But according to that procedure there it shows Enter your S7-200 connection as "Communication driver". Is it possible without S7-200 |
12/7/2011 1:00 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello, You can order Starter Package KTP600 Basiccolor PN (6AV6652-7DA01-3AA0)
Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 12/7/2011 1:07 PM |
|
12/10/2011 8:32 AM | |
Posts: 2930 Rating:
|
Hi, yes you can use a KTP600 PN to controll a LOGO! 0BA7. If you have't bought the HW up to know, then I recommend a LOGO! 0BA7 starter kit. Here the WinCC Basci V11 is part of the kit. You then only need to by the KTP600. A example how to program both (LOGO! & KTP600) you will find in the LOGO! application examples: www.siemens.com/logo Hope this helps |
4/18/2012 5:37 AM | |
Posts: 40 Rating:
|
Good morning Every body I purchased one HMI (KTP600) for connecting with Logo v7. I purchased this to create a programme as per the attached document. I am not well experienced in HMI with Logo V7. My Pc is installed with Logo soft comfort V7. What else I have to install to create a programme in HMI and how it can be configure. I can create programme in Logo soft comfort V7, Please help me to create programme in HMI. I want to make this HMI as an operating station instead of Logo TD Attachmenthmi_communication.zip (253 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on