4/29/2014 9:18 AM | |
Posts: 90 Rating:
|
Hi everybody! Please show me software and how to upload program from C7-626 panel. Thanks! |
4/29/2014 6:42 PM | |
Posts: 784 Rating:
|
Hello, The panel in C7-626 is based on OP25. So, there doesn't have options to make upload. Perhaps the attached file might help. Best regards.......... Attachment21907703_Back_transfer_devices_e.pdf (804 Downloads) |
Last edited by: Wago at: 4/30/2014 6:51 PMLast edited by: GrasserF at: 4/29/2014 10:42 PMdeleted link, inserted attachment |
|
5/11/2014 5:06 AM | |
Joined: 5/28/2008 Last visit: 7/30/2024 Posts: 4514 Rating:
|
C7-626is an old Compact product consists ofS7-300 CPU 315 2DP (128 KB), SIMATIC OP25 AND IM 360, 16 DI, 16 DO, 4 AI, 4AO, 4 UI. Here's manuals of the above product: As per above manuals, you can download or upload PLC program exactly like working with S7-300 systems using PG & Profibus programming cables. You can make your own Profibus programming cables using a bus connectors and profibus cable. You can use PC adapter as well. In the manual it's mentioned the part number of PC adapter serial type, but you can use PC adapter USB as well. Please note that this manual is an old manual. For programming a blank OP you have to use serial cable "6XV1440-2K..". This cable is no longer available for ordering but you can do it yourself. Here's bellow its pin assignment: Hope this helps. |
Ayman Elotaify |
|
5/11/2014 9:00 AM | |
Posts: 784 Rating:
|
Hello Ayman, Kindly review my previous attached file. Best regards........
|
5/11/2014 1:56 PM | |
Posts: 784 Rating:
|
Thanks Ayman Have a nice day.
|
This contribution was helpful to
1 thankful Users |
6/6/2014 1:34 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
I hope you have the original project to download it once again. Best regards, Hristo Mihalev |
6/6/2014 1:47 PM | |
Posts: 90 Rating:
|
I don't have original project. I have an other similar C7, it is operating. I want to backup program from it. Then downloading to this C7. I can do that? |
Follow us on