4/20/2016 9:59 PM | |
Posts: 8 Rating:
|
I understand that PC should take the place of Simatic500/505 in this pinout? Protool is freeware? |
4/21/2016 1:53 AM | |
Joined: 5/28/2008 Last visit: 7/30/2024 Posts: 4514 Rating:
|
Hello, Protool Pro is not a freeware. But it is an obsolete software from several years. When you get the Protool project from programmer, we have more than one solution. You can contact nearest Siemens representative to give you the Protool Pro. Or download the project to the OP7. OR you can send it to them and ask Siemens or any friend here if he have OP7 to download it to another OP7 and upload an image file for you. Then you will be able to download this image file using Prosave which is a freeware. OR You can migrate it to another Panel. Migrate it to OP77B and then migrate it to KP 700. Hope this helps. |
Ayman Elotaify |
|
4/21/2016 4:55 PM | |
Posts: 8 Rating:
|
Ok, now we´re trying to get the program, after that we´ll see how to download it. Thanks friends ! |
This contribution was helpful to
2 thankful Users |
4/25/2016 5:27 PM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating:
|
Hello, Nooo You need the HMI program"Protool file"to download it to the panel OP7 If they lost it ..... No way except start the programming from the begining. |
Eng.Mohamed Ibrahim |
|
4/25/2016 6:06 PM | |
Joined: 5/28/2008 Last visit: 7/30/2024 Posts: 4514 Rating:
|
Hello, From the first post and even title of this thread indicates that you have lost the OP7 program. Specially as per your statement in the first post that the OP7 gives you a message "Ready for Transfer". Actually, this message means that there is no software on the OP. __________________________________________________________
Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
4/26/2016 1:02 PM | |
Posts: 8 Rating:
|
Here´s the first image they sent me when this started. Sorry but I can´t add the second image here, don´t know how. |
Last edited by: NanoFer at: 4/26/2016 1:03:08 PM |
|
Follow us on