3/8/2006 10:34 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
The Alarm Control is programmed to display a maximum of 1000 alarms (http://support.automation.siemens.com/WW/view/en/1957448) The idea is that you should never need to look at more than 1000 alarms and if you do then the problem is not with WinCC, it is with the plant for generating so many alarms[:P] Remember that you can use the Selection toolbar button to filter the alarms displayed. I hope this will not cause you any problems. Let us know if it does and maybe someone can come up with an alternative solution. Regards, Salma |
3/8/2006 2:05 PM | |
Posts: 1084 Rating:
|
hi, As off wincc 6.0 there is no difference between the short term and long term archive. |
Follow us on