6/30/2009 8:06 PM | |
Posts: 2661 Rating: (279)
|
Did you run the OS Project Editor in the client project? |
7/2/2009 8:20 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi hero, when you cretae a Server/Client project all graphic pages are on the Server and Client picks them from Server, but sometimes you have to put on Clients few fles like start page too (depends from your configuration). "OS project editor", as well as Phantom75,creates everything Client needs to make project running and create layout page like you can see in PCS7 standard application. If you have different layout, all what you have to do is copy the start page on the client too (layout page and main page maybe). Regards |
7/2/2009 3:39 PM | |
Posts: 10 Rating: (0) |
Yes I mean't the Windows username/password. thanks |