10/26/2021 8:19 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS Forum Community. In so far as WinCC existing plants are to be extended, WinCC licenses (e.g. Powerpacks or additional runtime licences) are required in the corresponding version. However, WinCC licenses of versions V7.0, V7.2 and V7.3 are no longer listed in the relevant product sections of the Siemens Industry Mall. The order data are available as download within the still accessible original delivery releases: Delivery release SIMATIC WinCC V7.0 Delivery release SIMATIC WinCC V7.2 Delivery Release SIMATIC WinCC V7.3 WinCC licenses in V7.0 can no longer be ordered due to the product discontinuation for this version. An exception are the license upgrades from V6.x/V6.2 to V7.0 which are required for upgrades of WinCC systems for the intermediate step via V7.0. For system upgrades, licenses of version V7.2 can be used if necessary, see also: Version dependency of WinCC licenses Version dependency of WinCC Powerpacks. The product phase-out has already been declared for WinCC V7.2 and V7.3, but the licenses can still be ordered at present. Best regards, SIMATIC International Technical Support Hub |
Follow us on