12/27/2021 3:21 AM | |
Joined: 12/13/2014 Last visit: 6/13/2024 Posts: 144 Rating: (12) |
There is not one thread with all HW8.3 and corresponding software bugs, everything scattered on different posts here and there. Seems like 8.3 is so far buggiest LOGO ever, at least i don't remember so many issues with previous versions (on first 0BA8 FS:01 Softkey function is faulty). --- [ LWE 1.1.0 ]--- Address book on LWE1.1 Upload/Download page doesn't save entered values after closing LWE. Next run address book is empty again. LOGOSoft Comfort address book works. Update: After checking with different OS-es for my amusement under Linux address book works. Investigating shows, that address book items are stored to <LWE_Install_Directory>/etc/address.properties. I changed long time ago entire directory ownership, where LWE resides to regular user (myself) with permission to write here too. Under Windows installing LWE with administrator rights leaves permissions to state, where address.properties file can't be written by regular user. ---[ LWE 1.1.0 ]--- Randomly LWE1.1 crashes without any warning or explanation (luckily not very often) when saving project. At least doesn't damage project files, but some changes are lost. ------------------------------------------------------------------------------------------ |
Last edited by: WWEE at: 12/27/2021 03:28:46Last edited by: Jen_Moderator at: 12/27/2021 07:10:48New subject after splitting Last edited by: WWEE at: 12/27/2021 07:53:05Last edited by: WWEE at: 12/27/2021 11:53:57 |
|
12/27/2021 7:45 PM | |
Joined: 8/2/2018 Last visit: 12/16/2023 Posts: 302 Rating: (5) |
Your previous post is nothing wrong. Any problem that even expert in this forum can not help may be solved by open support request as used to be suggested sometime by forum expert.... My report of trend view axis no decimal points is not problem but just lack some feature only. Trendview can be using good and will be better if it can config decimal points on axis value. If it is called bugs then it is good to say in Concluded bugs post here. |
Last edited by: M111 at: 12/27/2021 19:48:16 |
|
Follow us on