7/1/2008 9:52 PM | |
Posts: 2661 Rating:
|
Are you triggering alarm messages that are embedded with process values? I think I have not understood your problem properly. |
7/5/2008 1:18 AM | |
Posts: 2661 Rating:
|
Can you post some screenshots of your program? I need to see how you are generating the alarms to find out the reason for your problem. Thanks. |
4/22/2009 2:25 PM | |
Posts: 1 Rating:
|
I’m also having this problem. I have also configured alarms in the PLCforanalog values. If thesignal is greater than thealarm limit, theni set the alarm bit "true"(to WinCC). In the Properties, "Tag/Action"of single message line (in WinCC alarm logging) I have entered the process value tag (the analog value)to be shownin combination with the alarm text, triggedby the bit. Since I’m notusing chronological messaging in my project, I Will try if this is a sync problem due to registry values : "CycleSetValues"= "00000000" // Acknowledge tags (default value 0) "CycleAlarms"= "00000000" // Alarm tag cycle (default value 0) "CyclePValues"= "00000003" // Process value tags (default value 3) http://support.automation.siemens.com/WW/view/en/24725737 I will try: "CycleSetValues"= "00000003" // Acknowledge tags (default value 0) "CycleAlarms"= "00000003" // Alarm tag cycle (default value 0) "CyclePValues"= "00000003" // Process value tags (default value 3) I will come back with the results Wish me luck.... |
Follow us on