4/22/2009 11:34 PM | |
Posts: 2661 Rating:
|
You need the licenses for operation. What do you mean by setting up redundancy in the usual way? Can you see the option for Multi-User when you click on new project in WinCC explorer in single user stations (as shown in attachment)? If yes, you should be able to setup redundancy. If no, you should install the WinCC server option from installation CD, first. The installation should notimpact the existing stuff (Data Monitor & Web Navigator). If this is a running plant, doing all this could be tricky... AttachmentMultiUser.pdf (146 Downloads) |
4/23/2009 9:11 AM | |
Joined: 4/5/2006 Last visit: 6/25/2024 Posts: 917 Rating:
|
Hi spacha, I agree Phantom75how setup redundancy, there isn't an usuall way and unusual way: exist ONLY a way to setup redundancy using "Redundacyselection in WinCCExplorer". Doesn't matter if you are using "WinCC Server" or "WinCC Single Station", redundancy has to be configured and works same way. Regards AttachmentRedundancy.zip (169 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on