8/19/2022 7:39 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
For better understanding, please attach motor nameplate snap here. |
8/19/2022 8:28 PM | |
Joined: 5/19/2013 Last visit: 9/20/2022 Posts: 4 Rating: (0) |
Unfortunately, there is no access to it. Foto Motor only. |
8/20/2022 1:25 PM | |
Joined: 3/27/2008 Last visit: 4/27/2024 Posts: 1098 Rating: (137) |
Enter Motor details: 400V, 0.79cos pi, 2540rpm, 11.0Ampere, 5kW, 87Hz. P1082, will be set to 2540rpm. Connect the motor in Delta. You are using an inverter capable of delivering, 11Amperes at 400V? Tractor Attachment87 Hz configuration.docx (679 Downloads) |
Last edited by: Tractor at: 08/20/2022 13:29:45Last edited by: Tractor at: 08/20/2022 15:45:43Tractor |
|
8/24/2022 4:08 AM | |
Joined: 5/19/2013 Last visit: 9/20/2022 Posts: 4 Rating: (0) |
Yes. Tractor, thank you very much! |
8/25/2022 8:14 AM | |
Joined: 3/27/2008 Last visit: 4/27/2024 Posts: 1098 Rating: (137) |
Cool Have you tried the motor? does it work? Tractor |
Tractor |
|
9/5/2022 8:37 PM | |
Joined: 5/19/2013 Last visit: 9/20/2022 Posts: 4 Rating: (0) |
Everything is fine, everything works. Thanks!
|
Follow us on