11/10/2022 9:57 AM | |
Joined: 3/11/2019 Last visit: 5/23/2024 Posts: 1433 Rating: (261) |
Hi, at least, it is not stated in the official manual as compatible, so i would assume, this is not possible. SIMATIC S7-1500 Software Controller CPU 1505SP (F/T/TF), CPU 1507S (F), CPU 1508S (F) Version 21.9regards sancurz |
Feedback appreciated, please rate |
|
4/14/2023 6:15 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi persuit, Especially the first download to a software controller can be a bit tricky. This is because you need to make sure that the settings on the IPC match the configuration in the TIA Portal project. This is especially true for the network interface settings. You should check the requirements listed in the user manual, or you can create a configuration file from TIA Portal and load the PC Station from that file. Kind regards |
Follow us on