4/17/2023 11:20 AM | |
Joined: 4/17/2023 Last visit: 3/28/2024 Posts: 5 Rating: (0) |
Hello, please, i am a student and i start in siemens logo.I would like to drive the AM2 AQ output so that it delivers me between 0-10v.I have nothing in input, no sensor.how can i program it?.THANKS ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/17/2023 12:38:44New subject after splitting |
|
4/17/2023 12:27 PM | |
Joined: 12/18/2014 Last visit: 5/18/2024 Posts: 33054 Rating: (4082)
|
Address 1072 is not possible. With Word, a maximum of only 849 is possible as an address. AttachmentWeb server address 1072 not possible.zip (360 Downloads) |
Last edited by: ixo65 at: 04/17/2023 12:32:52 |
|
This contribution was helpful to1 thankful Users |
4/17/2023 4:40 PM | |
Joined: 12/13/2014 Last visit: 5/16/2024 Posts: 137 Rating: (12) |
Enough to drive even an industrial panel-mounted 12V LED. Tried that. |
4/18/2023 7:30 AM | |
Joined: 4/17/2023 Last visit: 3/28/2024 Posts: 5 Rating: (0) |
Automatically please |
4/18/2023 12:25 PM | |
Joined: 12/18/2014 Last visit: 5/18/2024 Posts: 33054 Rating: (4082)
|
Maybe this help you. In attachment a possible solution. In the input of the analog output you need units between 0 - 1000. AttachmentAM2_AQ.zip (273 Downloads) |
5/18/2023 3:10 AM | |
Joined: 4/17/2023 Last visit: 3/28/2024 Posts: 5 Rating: (0) |
thank you so much |
Follow us on