9/7/2023 10:10 AM | |
Joined: 5/6/2022 Last visit: 5/14/2024 Posts: 420 Rating: (83) |
Hi KSASiem, I'm not sure what could be causing this but the problem may be related to the Windows scaling feature. When set to greater than 100%, this behavior can occur in TIA Portal, especially when moving the TIA window and dragging it to another area of the screen. In general, TIA Portal does not support Windows scaling. Set the scale to 100% and see if the problem goes away if the scale is set to a value other than 100%. To change the scale: Home > Settings > System > Display Can you try to see if it could be due to this? You can also restore the PG M6. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on