11/15/2023 12:24 PM | |
Joined: 5/30/2022 Last visit: 6/3/2024 Posts: 524 Rating: (86) |
Hi Mad4Swift, You cannot download event notifier, it does not have TRIAL version as you can see in the following link of the Industry Mall, it is a product that must be purchased: WinCC/Event Notifier V7.5 SP2, Option for WinCC V7.5 SP2 Once you purchase it the way to configure it you can find it in the following link: How do you install an e-mail notification with the WinCC/Event Notifier option? |
If this information really helps, you could use the Rate function. |
|
Follow us on