12/12/2023 11:50 AM | |
Joined: 9/7/2013 Last visit: 5/20/2024 Posts: 2 Rating: (0) |
Hello Experts, I am facing an issue on one of my sites, I have just finalized the commissioning of the WinCC SCADA system including a redundant Server and 2 Clients. Recently I have noticed that one of my Servers goes into a Fault state but keeps working as a standalone runtime as soon as the healthy Server goes off or goes into fault my clients get errors and cannot fetch pictures from the server which is absolutely correct. My concern is the Servers going to Fault State. I have read multiple threads and increased the memory of the SQL server as suggested on one of the threads but the problem still exists. After restarting the Servers they work properly and after a few weeks, the Fault state returns and disrupts the operation. We have gathered some diagnoses from the servers using SIEMENS Diagnostic Data Collector software. I am attaching all snapshots and diagnoses reports in the link below for you experts to review and maybe point me to where I can solve the issue. Error ID : 1012701 In Wincc Alarm Log ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/12/2023 12:11:09New subject after splitting and Link optimized |
|
12/15/2023 1:39 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello AutoGen_491614 Its not easy to say whats the reason, one could be that you have forgotten one of the basic configuration steps after installing (for example the lmhosts configuration): https://support.industry.siemens.com/cs/de/en/view/868014 But i would recommend to open a Service request at siemens Support Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on