3/28/2018 4:30 PM | |
Joined: 5/8/2016 Last visit: 2/15/2024 Posts: 167 Rating: (13) |
hey you can make the communication from the side of s7 1200 and use get and put instruction in 1200 program using TIA and no change will happens in s7 400 station . other words you will extract and put data to from to s7 400 you will use s7 connection over profienet as you will see in the pdf file attached , - configure s7 connection in s7 1200 station - make the connection to unknown device , putting the target ip address of s7 400 - map the memory area you will read/write using PUT/GET instruction in user program . find the attached pdf may that help . regards ahmed hamad Attachments7_conn.pdf (725 Downloads) |
Last edited by: elctro hamad at: 3/28/2018 4:32:16 PMA lot of potential remains |
|
2/16/2024 10:01 AM | |
Joined: 8/21/2014 Last visit: 11/13/2024 Posts: 1024 Rating: (14) |
New question published by AutoGen_7639394 is split to a separate thread with the subject Can't establish communication from 400-h to S7-1200 . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on