3/18/2024 2:42 PM | |
Joined: 8/23/2022 Last visit: 4/24/2024 Posts: 7 Rating: (0) |
Hi, I am using a Logo 8.4 "The following features are new for LOGO! 6ED1052-xxx08-0BA2 device: Variable Memory extension – VX: the extended area of V area, and it has the same memory function as V area; – VR: the extended area to store retentive data, and the behavior is the same with retentivity of function block. When you save the circuit diagram to the SD card, VR area values in the circuit diagram will be sychronized to the inserted SD card." I can't find the VR area. When it comes to storing to variable memory , under Range it gives me only V or Vx . Can anyone help? ------------------------------------------------------------------------------------------ |
Last edited by: andreas vouzikis at: 03/18/2024 15:34:28Last edited by: Jen_Moderator at: 03/19/2024 05:30:14New subject after splitting |
|
3/18/2024 4:11 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066)
|
|
This contribution was helpful to2 thankful Users |
3/18/2024 7:11 PM | |
Joined: 8/23/2022 Last visit: 4/24/2024 Posts: 7 Rating: (0) |
great! Thanks a lot. |
Follow us on