5/19/2024 5:58 PM | |
Joined: 1/11/2016 Last visit: 6/10/2024 Posts: 1 Rating: (0) |
Thanks for the explanations SSA with class 2 master. One point is still not clear for me even if this thread is quite old, but i am facing this situation right now. If I have Simatic PDM (class 2 master) connected to a PLC 1517 Profinet interface, so the PLC is working as a S7 Datasetgateway, is it then possible to use SSA function for chaning the DP address of the underneath laying PA Slaves (there is a CM1542 and DP/PA Coupler connected also) or is it then blocked, because the route is going through the class 1 master (PLC)? At the moment we can read online values via PDM but we cannot change the DP address. Would really appreciate a clear answer to this to sort the problem soon. Thanks, Matthias ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/21/2024 11:05:29New subject after splitting |
|
Follow us on