8/24/2009 1:41 PM | |
Joined: 3/27/2008 Last visit: 4/30/2024 Posts: 1099 Rating: (137) |
I use a 232 to 485 converter which was produced for the Micromaster 410, this is useful for connecting to Micromasters whilst the keypad display is fitted. When using this connected to terminals 29/30 on the MM440 you are using 'serial Interface COM link', so this is where the baud rate can be set, P2010:0. If you do not have a serial port this works with a usb to 232 converter. AttachmentA5E00150456A2_17521975_MM410_to_PC_Connnection_Kit_A2.pdf (324 Downloads) |
Tractor |
|
This contribution was helpful to1 thankful Users |
Follow us on