10/20/2009 10:50 AM | |
Posts: 15 Rating: (0) |
Hi Mike J, i have attached my pdl and a prt screen. i have created from the standard slider object the following. input on iofield is floating point, i read the input value an change it to integer before writing to process value, as you can see in the Input event of the IOField. the slider works with integers. If you select both objects and change the tag link where the TAG FREQ is in your own tag (INTEGER) you can change the value whith the slider, or on the input field with a floating point value set to a max of 60.0 . Hope you see wats the problem for mee. Nesnaj AttachmentExample.zip (130 Downloads) |
Follow us on