1/27/2010 1:59 PM | |
Posts: 65 Rating: (0) |
Hi, it is possible to use CFC with PN-CPU? It's released? Dennis |
1/28/2010 8:46 AM | |
Joined: 10/7/2005 Last visit: 5/19/2024 Posts: 3005 Rating: (1048)
|
Hello Deka I must admit I haven't tested that one yet, but it surely must be possible to use CFC with a PN-CPU. At the end of the day CFC is "just" another language option which can be used to programa S7 PLC's and will compile down to STL code (via SCL as an intermittent Step for that matter, the SCL compiler is part of the CFC option package). Anyway, lastest CFC version is V7.1 SP1 (useable as of Step7 V5.3) and you can find out more about itat the link below which also contains the all import readme file: SIMATIC CFC V7.1 + SP1 I hope this helps |
Cheers |
|
Follow us on