3/12/2009 1:29 AM | |
Posts: 2661 Rating:
|
Hi, |
This contribution was helpful to
1 thankful Users |
3/12/2009 2:38 PM | |
Posts: 12 Rating:
|
I should have been more specific on installed software. S7-PLCSIM v5.4 + SP1 Revision No.: 5.4.1.0 All Step 7 software is SP1. |
7/13/2009 5:12 PM | |
Posts: 5 Rating:
|
Hello. I just have the same problem now. I ve installed STEP7 V5.4 SP4. After installation i realized PLCSIM was not included (is this normal? So far i have thought that PLCSIM was a small part of STEP7. Was i wrong?) and thus PLCSIM was not installed. Also Automation License was not included. I installed PLCSIM V5.4 and Automation License Manager V4.0 SP2 then. Still after this no download from the SIMATIC Manager is posible. I've tried also installing PLCSIM V5.4 SP2 and PLCSIM V5.4 SP3. I tried to install first PLCSIM but the system tells me i must have intalled SIMATIC at least. Any help is very apreciated. Thaks in advance. AttachmentSCREENSHOTS.zip (600 Downloads) |
7/23/2009 8:19 AM | |
Joined: 5/14/2008 Last visit: 9/4/2024 Posts: 19 Rating:
|
Keep the PG/PC interface as PC Adapter(MPI) and try it will work. |
Follow us on