6/15/2011 7:04 AM | |
Posts: 2661 Rating: (279)
|
What you say istrue but for the problem reported in this thread you do not want to change the block numbers of the standard library blocks. These problems typically occur when you "mix" blocks from different libraries. For example if you migrate your old project without upgrading to new library and then insert blocks from new library. The option is available to either stay with the old library or upgrade to the new library. But this should be planned beforehand. All the steps for migration are described well in the following links: Software update with utilization of new functions (PCS 7 V6.x or higher to V7.1) Software update without utilization of new functions (PCS 7 V6.x or higher to V7.1) Regards |
This contribution was helpful to1 thankful Users |
Follow us on