9/13/2005 4:10 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating:
|
Dear Mr Gnani , Maybe one possibility is to use the latest chipset driver for your Field PG. (Via Hyperion 4 in 1 driver) You can download this driver at http://www.viaarena.com/?PageID=2 A later driver for the ethernet adapter (as you have at your Backup CD) doesn't exist. The problem is that the pegasus software seems to be compatible to the via rhine ethernet adapter. But we can't do anything against it. A solution is to use the pcmcia network adapter as you described. Best regards Your Technical Support for Automation & Drives Oliver Koch SIEMENS AG |
Follow us on