12/25/2011 10:23 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
Assuming that you have wired DI - 1 for RUN and DI - 2 for Fault Acknowledge Now in this case set following P700-2 (Command from Terminal-Hardwire) P701-1 (DI-1 as RUN Command) P702-9 (DI-2 as Fault Acknowledge) P1000-3 (Set Fixed Freq as Setpoint) P1001- 15 (Set freq at which you want motor to drive) P1016-1 P1020-1 I hope this will help you out Please refer MM430 Operating Instruction and Parameter List Manuals Regards Devesh |
Last edited by: Vithani at: 12/25/2011 10:26 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
Follow us on