4/12/2012 3:44 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Hello Everybody I don´t know if this question is here or maybe in Communication/Networks. Sorry if I am wrong. I have a issue that I don´t know how to solve. Righ now I´m working with CP340 RS232 , my system is Windows 7 32bits The problem is that I can´t configure the CP, because the button properties is disable. Look at the attachment. If anyone can help me. Thanks |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/12/2012 4:11 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Installation of Point-to-Point options package(: 27013524) is necessary. Best regards, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
4/12/2012 4:26 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
It´s works perfectly Thank you very much! |
Last edited by: JM76 at: 4/12/2012 4:34 PMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on