4/16/2012 2:59 PM | |
Posts: 303 Rating: (3) |
Hi All, This is saradhi. I am facing problem while communicating s71200 PLC with s7-200 PLC. I can get and put values into s7-1200 by using s7-200. i.e, in the ethernet wizard of s7-200 i made s7-200 as a client and define data transfers. I put TSAP of remote system is 03.00. With this i am able to write and read values from s7-1200. But i am unable get read and write operations from s7-1200 to s7-200. i used the blocks T_SEND and T_RECEIVE in s7-1200 for communicating with s7-200. and i am also insert new connection in s7-200 as SERVER. i am including both the configuration files. Please help me regarding this.
AttachmentS7-200 With S7-1200.zip (64 Downloads) |
5/11/2012 10:54 AM | |
Posts: 303 Rating: (3) |
It is possible |
5/11/2012 11:13 AM | |
Posts: 378 Rating: (47) |
Hello, does this mean your problem is solved? And if it is solved, how did you solve it? Best regards Bilao |
5/11/2012 11:17 AM | |
Posts: 303 Rating: (3) |
It is possible through Profinet protocol. for this i am configure Get and Put blocks in s7-1200. |
This contribution was helpful to1 thankful Users |
Follow us on