10/17/2012 3:00 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665)
|
Hello Mr. Hirsch; Translation from the German (thanks to Google Translate):
Mr. Hirsch, you seem to have posted in the English section of the forum by mistake, switch the languageselection at the ntop of the forum page if you ould like to repost in the German section. Meanwhile, have a look at the following ApplicationNote: Directly controlling a MICROMASTER 4 / SINAMICS G120 / SINAMICS G120D from a SIMATIC HMI station via PROFIBUS-DP and PROFINET It discusses controlling a MM440 through Profibus (and Profinet) with a CPU 315-2DP and a TP 177B, so it should be close-enough to what you are trying to implement. And it is available in German... Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on