2/28/2013 11:10 AM | ||||||
Posts: 1530 Rating:
|
Hello mohamedsamy, IfWinCC is installedonyour computers you don't have to install anything from connectivity pack on the system. The WinCC OLE DB Provider is installed with every normal WinCC installation. Mentioned "Station V7.0 Upgrade"is part of WinCC Basis Upgrade, so you don't have to install it separately. You only have to install Connectivity Pack client or server, when there is no WinCC installation on one of your computers. Connectivity Pack includes Connectivity Station You need the Connectivity Pack License on the computer where you want to access the WinCC data. If you want to access WinCC data of both computers you need two Connectivity Pack licenses. The license activates the WinCC OLE DB Provider on the system. Best regards Bizur |
|||||
This contribution was helpful to
1 thankful Users |
Follow us on