6/23/2013 4:08 PM | |
Joined: 3/25/2013 Last visit: 3/23/2023 Posts: 4 Rating: (0) |
Hi, on T3000, AUMA have HW-proxy module in libraray. For T2000 I'm not sure but this is my opinion: For sure youwill need Y-link to convert redundant profibus to single profibus. Y-link have limitation regarding to amount of data you want to send/receive. Also I'm not sure if u can use Y-link on same profibus line where FUM racks are connected (possible usage of 443-5 extended profibus cards - only if u use S7-400 cpu). If T2000 doesn't have AUMAproxy in library then you will have to use generic profibus deviceproxy and GSD files (how exactly I'm not sure). Check AUMA site for network. Each AUMA is slave with individual slave number. Pleasefind somedata for AUMAin attachment. BR, AttachmentAUMA.pdf (473 Downloads) |
Last edited by: O_Moderator at: 6/25/2013 3:35 PMLast edited by: CS Moderator at: 6/25/2013 11:03 AMAttachment reattached Last edited by: Dr@gonfly at: 6/23/2013 4:25 PM |
|
Follow us on