7/15/2013 7:50 AM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating: (188) |
Hey Phantom75, where did you find the info above? I don't find this in WinCC Information System |
B r g d s , |
|
7/16/2013 1:03 AM | |
Posts: 2661 Rating: (279)
|
Hi Tornes, See the following FAQ's regading the extended analog display and extended status display: Implementing and configuring the extended analog display with SIMATIC PCS 7 V6.x How do I use and configure an extended status display with SIMATIC PCS 7? For configuring alarms you use the eventstate tag in the Group value attribute. The evenstate tag is generated by an alarm block (Alarm_8P for example)in the S7 program. If you do not want to use eventstate then you have to conditionally trigger the bits in the Group value attribute, for example bit 31 will generate an Alarm High. Clear as mud? Regards |
This contribution was helpful to1 thankful Users |
Follow us on