9/9/2013 3:02 PM | |
Posts: 19 Rating: (0) |
Dear All, In my Project , I need to communicate two RTU's with Central WinCC SCADA 7.0 for Monitoring & Control Purpose. RTU's are standalone system with S7-400H + ET 200M Redundant bundle+ CP 341 with Modbus Slave Driver. CP 341 Modbus RTU is converted to Modbus TCP/IP with suitable Converter and transmission through GSM Network [ Modbus TCP/IP to GSM Gateway] Now On WinCC Side, Shall I able to configure both Modbus TCP/IP Slaves directly or I need OPC Server. Thanks in advance. AttachmentWinCC Modbus TCPIP Comm with Slaves.pdf (331 Downloads) |
Last edited by: M Saad Khulsai at: 9/9/2013 3:03 PM |
|
Follow us on