10/5/2013 1:27 AM | |
Posts: 2 Rating: (0) |
Are parameters available via the front panel without use of a laptop?Is there a procedure to access them? I need to find value of P2106 |
10/5/2013 9:00 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Try with P0003 = 3 |
10/5/2013 9:07 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, And of course download the manual: Operating Instructions: MICROMASTER 440 0,12 kW - 250 kW Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on