9/15/2013 2:34 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Hello, If the response of your system is not satisfactory, it is because FB41 is not designed for such an application.FB41(CONT_C) can be used to control process via continuous input and commands via continuous outputs.More information and samples are available here: PID Control Package - FB41 Samples Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 9/15/2013 2:38 PM//typo |
|
10/14/2013 12:12 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
Tricks for base settings and fine tuning published by autobotis split to a seperate thread with the subject Regulation - tricks u can use to make a base setting and then do some fine tuning |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on