11/16/2012 5:37 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello Dhiyia; The following lik provides an application note from Siemens that should answer your questions: How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)? This application note will not show you how to change the settings or the commands to the drives, only to read messages: In this FAQ we describe how to read out all error and warning parameters from a frequency converter of the SINAMICS/Micromaster family and display them on a panel. A library has been created in WinCC flexible for the error and warning messages. This FAQ gives a detailed description of how to establish a direct connection between a converter and the panel via PROFIBUS.
|
Last edited by: dchartier at: 11/16/2012 5:41 PM |
|
11/16/2012 6:30 PM | |
Posts: 56 Rating: (1) |
Dear dehartier Thank u for your usefull reply ... socan i use KTP600 DP or TP177B ... ??? Thank u ... |
12/19/2012 2:12 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can follow this link. How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)? This link describes how you communicate with a Panel to Micromaster about Profibus. Tweety |
1/11/2013 4:22 PM | |
Posts: 3037 Rating: (192)
|
Hello, Perhaps you can find it manual of the MM420. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csSearch&objaction=cssearch&lang=en&siteid=cseus&query=&query2=MM420&content=adsearch%2Fadsearch%2Easpx Tweety |
8/17/2015 3:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on