11/20/2015 11:12 PM | |
Posts: 7 Rating: (3) |
Hi, I have a program that controls my heating in my garage(08BA). By a potentiometer I set the desired temperature at a analogue threshold trigger block. A PI and PWM block is switching the heaters on/off and all works fine. I can connect to the LOGO by internet and see the hour counter and actual set point. Now to the question - is there any possibility to offset the input value remotely? I want to connect to the LOGO by internet and offset the set point. Lets say the potentiometer is set to 8 degrees and I want to set the value to 12 degrees by my smartphone. Is itpossible? See attached my program. Regards Stefan AttachmentClosed-loop control and pulse width modulation Stefan.lsc.zip (134 Downloads) |
11/21/2015 7:53 AM | |
Joined: 12/18/2014 Last visit: 6/13/2024 Posts: 33192 Rating: (4105) |
I've adapted your program that you can change the setpoint via the display. This no longer need the analog input with the potentiometer. So you're then able to change the setpoint via the web server. Explore the Video. AttachmentTest.zip (137 Downloads) |
This contribution was helpful to1 thankful Users |
11/21/2015 10:21 AM | |
Posts: 7 Rating: (3) |
Thanks a lot! |
This contribution was helpful to1 thankful Users |
Follow us on