4/28/2016 4:54 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello All We are facing a problem in a WinCC 7.2 Project with OPC Channel. We have configured an OPC Channel connection to Yokogawa DCS System. ( Yokogawa is Server ). We are able to browse the Tags of Yokogawa DCS and insert the same into WinCC. However when we are putting the system in Runtime, we are getting connection Error. The Error Logs are attached. Can anyone advise what exactly could be the issue. Thanks Navnag AttachmentOPC_Logs.zip (140 Downloads) |
There is no such thing as the last bug in a program |
|
5/3/2016 3:25 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello I found the following guide which explains in very simple terms, How to troubleshoot a OPC connection : OPC & DCOM Troubleshooting: Quick Start Guide Also found this tool, which is a great help in diagnosing OPC connection problems OPC Expert I could solve the problem of connection with the help of these two. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to3 thankful Users |
5/9/2016 1:35 PM | |
Posts: 457 Rating: (46) |
Thank you for your help with OPC Connection. |
Follow us on