4/7/2017 11:02 AM | |
Joined: 7/14/2014 Last visit: 3/28/2024 Posts: 6 Rating: (0) |
Hello, I have a problem with INFO dialog in faceplate. On the Server, ES, Clients and Web Server it working perfectly but on the Web Client when I click on the "Info" button on faceplate, WinCCViewerRT.exe (or ControlHost.exe if using IE) is crash. It appeared after I filled User Archive C_INFO on the server. When C_INFO was empty, "Info" dialog on the Web Client was opening without crash with points only in fields. I did recommendations about start RegCtrlsWEB.bat to register CematRichEditControl.ocx, no result. I need help!
CEMAT v8.0 SP1 (007 - Heidelberg Cement) AttachmentScreen Shots.pdf (38 Downloads) |
Follow us on