1/29/2012 12:57 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, Let me say here the differences between BOP & AOPs.
Now back to your questions:
Yes. And also BOP is a 5-digit display while AOP is multiline display with description of parameters.
From Part numbers.
Using software starter/ drive monitor, you can keep parameters saved on your PC. |
Last edited by: Ayman Elotaify at: 1/29/2012 12:59 PMAyman Elotaify |
|
1/30/2012 1:13 PM | |
Posts: 32 Rating: (0) |
Adddition to above post ; |
1/30/2012 2:22 PM | |
Joined: 4/24/2006 Last visit: 4/30/2024 Posts: 8626 Rating: (1147) |
Hello panthripu, When you get message "Out of Memory" you will have to delete some Languages you do not need. See also this thread: /tf/WW/en/Posts/17665 From manual: Memory Limitation The delivered AOP supports five European Languages of English, German, French, Spanish and Italian. Due to internal memorylimitations the user should delete one of these languages in order to upread the specified ten parameter sets that can be held on the AOP. To Delete a Language Select “Language” from the top level menu, highlight the language you want to delete then press “Fn” and “↑”. Please note thatonce a Language has been removed it cannot be restored. Best regards, Wizard |
1/30/2012 2:26 PM | |
Joined: 4/24/2006 Last visit: 4/30/2024 Posts: 8626 Rating: (1147) |
Dear panthripu, Please have a look at this link: What different connection arrangements are possible with the optional Operator Panel and communication Options for the MM4 inverter? PC to MM4 Connection Kit (6SE6400-1PC00-0AA0): Best regards, Wizard |
2/16/2018 10:56 AM | |
Joined: 6/19/2017 Last visit: 4/30/2024 Posts: 7993 Rating: (163) |
New question published by safaa2 is split to a separate thread with the subject Searching for some parameters on the expert list of the micromaster440 . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on