2/17/2018 5:29 AM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
So I have been wanting to use the math instruction block which would suffice for fragmented data definitions at start up. The real issue is now, the block only accomodates integer not floating point. Does that mean I have to fake the floating point by padding and dividing? Ive added a spreadsheet schema which is part of setting up eg in this case a simple water dosing algorithm with scaling coefficient. What is the most elegant way to achieve a parallel concept in FBD? ie predefining constants and doing some preuse maths on various vectors? AttachmentWater System - Schema.pdf (136 Downloads) |
Last edited by: Image_Engine at: 2/17/2018 5:30:34 AM |
|
Follow us on