10/18/2018 7:52 AM | |
Joined: 8/24/2018 Last visit: 6/23/2022 Posts: 3 Rating: (1) |
Requirement Execute NC programs in MCD without PLCSIM Advanced to validate programmed motion. Challenge MCDs Runtime NC functionality only works in combination with Machine Tool Builder. How to run NC with MCD only. Known Workarounds
Usage of CAM Profiles for each Axis. Concept: one CAM profile per Axis (X,Y,Z). A VirtualAxis to sync CAM Profiles to. Master of CAM Profile is the VirtualAxis. Slave is the movement of the axis from the G-Code. Workflow:
Simple RTB that positions axes according to coordinates defined in an array. Workflow:
Are there any other/simpler methods for running NC code in MCD? AttachmentNCcode.zip (883 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on