12/22/2018 5:24 PM | |
Joined: 6/22/2015 Last visit: 5/21/2024 Posts: 20 Rating: (0) |
Dear all, I need to know which CPU suitable for Oil & Gas and Ambient temperature 70 degree celcisus for critical plant (Redundant CPU)(H2S Gas Plant..) Here I have suggested the below attachement file and Architecture , i have doubt in this below system whether its suiable or not for the requirement. knidly give me the valuable suggestion for my clarification. SIPLUS S7-400 CPU 412-5H and Distributed system with SIPLUS ET 200SP IM155-6PN STANDARD through profinet communication. Thanks & Regards, Ganesh Pandi Attachment400_TEST.xlsx (119 Downloads) |
Follow us on