10/16/2019 10:08 PM | |
Joined: 10/16/2019 Last visit: 7/23/2020 Posts: 2 Rating: (0) |
Hi, Marcjan! If it's available only the three phase (L1, L2 and L3), neutral (N) is not in this scenario.... Is it possible power on Logo 230RC and DM8 module with two phases (L1 and L2, considering L2 "as reference")? Thanks!
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/17/2019 08:32:58New subject after splitting |
|
10/17/2019 5:04 AM | |
Joined: 12/18/2014 Last visit: 6/26/2024 Posts: 33242 Rating: (4112)
|
You can connect the inputs of a 230V LOGO! or 230V extension modules with different phases, but only in groups of 4 four inputs. See attachment. It's an excerpt from the manual. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 48.pdf (544 Downloads) |
Follow us on