2/1/2020 1:30 AM | |
Joined: 1/20/2010 Last visit: 8/3/2021 Posts: 5 Rating: (0) |
Hello, Could you please explain to me what will happen if the reference value for the torque in Drive data in Technology object configuration in TIA portal is different from real value of torque data on the name plate of the motor. For example I setted reference torque in TO in TIA portal 3.5 Nm and real torque is 35 Nm? And if I go to the Starter there I can see values like you described in text before. I hope so that somebody will see this question, because the post is very old :) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/03/2020 06:42:56New subject after splitting |
|
Follow us on