5/19/2020 1:18 PM | |
Joined: 10/10/2017 Last visit: 1/7/2024 Posts: 59 Rating: (0) |
Yes, in this case, I have done the hardware configuration, and commissioning and programming using Simotion Scout. |
5/19/2020 1:30 PM | |
Joined: 10/10/2017 Last visit: 1/7/2024 Posts: 59 Rating: (0) |
Is this correct? I could not find "Activate IO Device mode", only "I-device mode". Should other boxes below be checked? |
5/20/2020 8:25 PM | |
Joined: 10/10/2017 Last visit: 1/7/2024 Posts: 59 Rating: (0) |
Hi, I have done all the listed steps from configuring PROFINET addresses and I have downloaded script for generating GSDML from this site https://support.industry.siemens.com/cs/document/92022677/sinamics-g-s%3A-generating-gsdml-files-for-s120-s150-g130-g150-s110?dti=0&lc=en-DE Is there anything I can do to generate GSDML file? |
5/22/2020 8:13 AM | |
Joined: 5/12/2006 Last visit: 6/14/2024 Posts: 22263 Rating: (2989)
|
in step7 hw config options you can generate the gsd file |
Follow us on